How can we help you today?

Is it possible to program a Twido PLC through the 499TWD01100 TwidoPort Ethernet TCP/IP interface module?

NOTE that the Twido range is obsolete, closely replaced by the M221 series of PLCs. You can convert the old TwidoSuite program to the new Ecostruxure Machine Expert Basic software for use with the new PLC.

Yes it is possible to program a Twido PLC via the TwidoPort Ethernet interface module.


When configuring an Ethernet connection to a PC in TwidoSuite, the Modbus address defaults to ‘direct’.  This needs to be changed to match the address of the Modbus port of the Twido as the connection between the ethernet module and the PLC is via Modbus.

To find or alter the Modbus address of the Twido serial port, select the ‘describe’ tab in TwidoSuite, double click on the communication port of the Twido PLC and select an appropriate address (in the example below it is set to address 1).

Create a new Ethernet connection by clicking on the ‘preferences’ icon in the top right hand corner of TwidoSuite.
How to create new ethernet connection

Scroll down to the connection management table and add a new connection (or modify if you have an existing Ethernet connection configured).  Select the connection type as ‘Ethernet’, enter the IP address of the TwidoPort, (FAQ, FA166803 describes how to assign an IP address to a TwidoPort) and select the appropriate Modbus address in the ‘Punit/Address’ column (1, in our example). See below;

connection management table

Using this new connection, you will be able to communicate to the Twido PLC via the TwidoPort module.

communication demonstration

Schneider Electric UK
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
  • Help and contact centre
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
  • General Terms of Business
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings
  • Preference Center