Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the Acti 9 incomer switch SEA9NI1603 or SEA9PNI1603 have a Undervoltage release or Shunt trip coil fitted?

No the SEA9NI1603 CANNOT have a Undervoltage or Shunt trip coil fitted.

With one exception none of the Switched disconnectors for the B Type boards can have Undervoltage release coil, Shunt trip coil, or Auxiliaries fitted. This is because they are based on the Interpact INS range.

The only Acti 9 switch incomer that can have a Under voltage release or Shunt trip coil fitted is the SEA9NI2254 as this is based on the NSX range

Switched Disconnector
for B type boards
Possible
Undervolt
Shunt Trip
Auxiliary
SEA91253NNo
SEA91254No
SEA9NI1603No
SEA9NI1604No
SEA9NI2003No
SEA9NI2004No
SEA9NI2254Yes
SEA9NI2503No
SEA9NI2504No


This includes the Acti 9 Isobar P incomers, such as SEA9PNI1603 or SEA9PNI2503 etc. The part number which can have these coils are the SEA9PNI2254 and SEA9PQ2254.

Schneider Electric UK

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and contact centre