Issue:
EZM application
Product Line:
EZM Meter Pak
Resolution:
Devices with 800 A Main Horizontal cross bus can be connected with devices that contain 1200 A Main Horizontal cross bus, BUT there are some restrictions see FA121813 for when a EZM Main Must be center mounted within the overall loading of a line up.
EZM application
Product Line:
EZM Meter Pak
Resolution:
Devices with 800 A Main Horizontal cross bus can be connected with devices that contain 1200 A Main Horizontal cross bus, BUT there are some restrictions see FA121813 for when a EZM Main Must be center mounted within the overall loading of a line up.
Released for: Schneider Electric USA