{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
What is the part number for a field installable 120kA per phase TVSS unit for an I-Line panel?
120/240VAC, 1PH, 3W: FC1IAM12
208/120VAC, 3PH, 4W: FC2IMA12
480/277VAC, 3PH, 4W: FC4IMA12

NOTE: 13.5`` of branch mounting space is required. Cannot be installed in HCN interiors.


Revised 3/10/04






CTA-ID : 2007678

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.