Issue:
Product Design Features
Product Line:
EZM metering and Meter-Pak metering
Environment:
Device Mounting
Cause:
Application
Resolution:
There are NO Flush mount or Semi-Flush mount EZM metering devices, They are all considered Surface mount.
There are NO flush mount MP devices, BUT the MP devices can be Semi-Flush mounted with the correct Semi-Flush Flange Kit(purchased separately). SEE THE CURRENT ON-LINE DIGEST FOR KIT PART NUMBERS.
EXCEPTION: THE MPL.... Meter-Pak devices CANNOT be Semi-Flush mounted, they are surface mount ONLY.
Product Design Features
Product Line:
EZM metering and Meter-Pak metering
Environment:
Device Mounting
Cause:
Application
Resolution:
There are NO Flush mount or Semi-Flush mount EZM metering devices, They are all considered Surface mount.
There are NO flush mount MP devices, BUT the MP devices can be Semi-Flush mounted with the correct Semi-Flush Flange Kit(purchased separately). SEE THE CURRENT ON-LINE DIGEST FOR KIT PART NUMBERS.
EXCEPTION: THE MPL.... Meter-Pak devices CANNOT be Semi-Flush mounted, they are surface mount ONLY.
Released for: Schneider Electric USA