Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the part number for the Heatsink Fan for FLEX58U90M2, FLEX58D12M2, FLEX58KU90N4, FLEX58KD12N4, FLEX58KD16N4 or FLEX58KD23N4?
Issue:
Heatsink fan part number for Flex drives.

Product Line:
ATV58 Flex

Environment:
FLEX58U90M2, FLEX58D12M2, FLEX58KU90N4, FLEX58KD12N4, FLEX58KD16N4 and FLEX58KD23N4.

Cause:
Heatsink fan replacement

Resolution:
The part number 31158-067-50 is the fan assembly only. This can be used if replacing a failed fan if the other hardware is in good condition.

The part number 31158-296-50 is the fan assembly, jumper wires, gaskets and instruction sheet. This part should be ordered if getting a fan kit for a new installation of a FLEX58 drive into an enclosure.

These are not the same fan kits that are used for the ATV58 type H and type FVC products.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings