Issue:
Product Features
Product Line:
QO and Homeline Load Centers
Resolution:
There should be no limitation other than the amount of termination openings on the PKxxGTA equipment ground bar. One LK100AN lug kit will require 3 adjacent terminals available on the PKxxGTA ground bar for mounting.
Product Features
Product Line:
QO and Homeline Load Centers
Resolution:
There should be no limitation other than the amount of termination openings on the PKxxGTA equipment ground bar. One LK100AN lug kit will require 3 adjacent terminals available on the PKxxGTA ground bar for mounting.
Released for: Schneider Electric USA