Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are Weathershields available for older Sorgel/Square D Ventilated Transformers?
Issue:
Weathershields for older Ventilated Transformers

Product Line:
LV Transformers

Environment:
Applies to Low Voltage Transformers from SquareD/Schneider Electric

Cause:
Older Sorgel Transformers

Resolution:

Some very old Sorgel/Square D Ventilated Transformers had enclosures that were different in size than those used on newer Transformers.  Unfortunately, these obsolete enclosure types do not have Weathershields available from SquareD/Schneider Electric, even though the catalog number may be the same for both old and new Transformers, i.e. 75T3H, etc.  Before ordering a Weathershield, measure the width of the older Transformer and be sure it is the same as the width of the current enclosure and corresponding weathershield as listed in the Digest.


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings