What are the repair parts for the H463DS, series F6? (may be shown as F06)
Product Line:
Heavy Duty Safety Switch
Resolution:
The repair parts for the H463DS, series F6 (F06) are as follows. No other parts are available. (NOTE: Descriptions below of "left side" and "right side" mean your left or right as you face the switch)
-Line Base - one each of 4056776350 (left side base), 4056775750 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included)
-Load Base - 4056609550 (1 required for left side and 1 for right side)
-Line & Load Base mounting screw - 4020515101 (3 for each line base and 2 for each load base)
-Arc Suppressor Assembly - 4056635550 (1 required for left side and 1 for right side)
-Arc Suppressor mounting screw - 4020514501 (1 required per arc suppressor)
-Lug Assembly - 4025101851 (per lug)
-Lug Mounting Screw - 4020514202
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322802 (2 required)
-Lockplate mounting screw - 2194918121 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801
-Fuse Pullers - FPK0610 (1 required for each line base)