Issue:
Can Powerpact breakers be tested with the universal tester UTS3?
Product Line:
Powerpact Circuit Breakers
Resolution:
No. Secondary injection testing of these breakers would require the full function test kit S33595 or the handheld test kit S33594 for Powerpact P and R-frame breakers, or UTA tester STRV00910 for Powerpact H, J, and L-frame breakers.
Can Powerpact breakers be tested with the universal tester UTS3?
Product Line:
Powerpact Circuit Breakers
Resolution:
No. Secondary injection testing of these breakers would require the full function test kit S33595 or the handheld test kit S33594 for Powerpact P and R-frame breakers, or UTA tester STRV00910 for Powerpact H, J, and L-frame breakers.
Released for: Schneider Electric USA