Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the deadfront part numbers for an NF454L4 or NF454L4C interior?

Issue:
What are the deadfront part numbers for an NF454L4 or NF454L4C interior?

Product Line:
Panelboards

Environment:
Replacement parts

Cause:
Damaged or missing

Resolution:
Each panel requires the following deadfront Trims
(1) 80113-178-50 MLO Cover
(1) NFRPL454L4 Branch Section
(1) 80113-182-50 Load End Cover


NOTE: P/N 80113-178-50 (MLO Cover) & P/N 80113-182-50 (Load End Cover) are not available as individual parts, but are included with the NFRPL454L4 Branch breaker Deadfront

















Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings