Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are panelboards CAD (PBA) drawings listed in inches or millimeters (metric) dimensions?
Issue:
Panelboard drawings listed metric dimensions

Product Line:
Panelboards

Environment:
Products sold and used in North America

Cause:
Product Features

Resolution:
The panelboard CAD (PBA) drawings are `soft metric` which means that the all dimensions are given in inches and millimeters (mm).

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings