Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
When using an EZM main breaker or fusible switch as the utility main, can an EZM main terminal box be used as a branch feeder?
Issue:
Can the EZM main terminal box be used as a branch feeder on the other EZM main devices?

Product Line:
Metering Product

Resolution:
Yes, it is permissible to use an EZM main terminal box as a branch feeder to a downstream load if the main bussing of the utility main device is the same amperage or higher as the terminal box being applied as the branch feeder.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings