Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How can ground fault protection be added to the C60 Multi 9 circuit breakers?
Issue:
GFP and RCCB availability for Multi 9 breakers and supplementary protectors

Product Line:
DIN Rail Mounted Circuit Breakers

Resolution:
To add ground fault protection to Multi 9 circuit breakers, a UL1053 listed ground fault protector (GFP) or IEC61008 listed residual current circuit breaker (RCCB) must be wired in series with the Multi 9 breaker or supplementary protector.  These devices offer equipment protection at 30 mA, 100 mA, or 300 mA.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings