Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for the rotary handles for the PJL and MJL breakers?
Issue:
Part number of Rotary Handle for PJl and MJL Breaker

Product Line:
Powerpact breaker Accessories

Environment:
Rotary Handle

Resolution:
The rotary handle is available factory assembled only on the PJ frame breakers. The suffix for these is: RD10 directly mounted, or RE10 door mounted, for a standard black handle. There are no rotary handles available for the MJ style breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings