Video: Can I get the bag of hardware supplied with the DASK Transformer lug kits?
Issue:
Content of Transformer lug kits
Product Line:
LV Transformers
Environment:
Applies to Lug Kits for Transformers by SquareD/Schneider Electric
Cause:
Lugs require nuts and bolts to attach them to the Transformer terminals
Resolution:
The components of the kit (including the hardware) are not available on an individual basis from SquareD/Schneider Electric. Refer to Digest 178 Page 14-9 Transformer Lug Kits table. This table lists the quantity and size of hardware supplied, which can be obtained at any local supply store.
The following video describes the contents of the DASKGS250 & DASKGS400 Transformer Lug Kits:
Content of Transformer lug kits
Product Line:
LV Transformers
Environment:
Applies to Lug Kits for Transformers by SquareD/Schneider Electric
Cause:
Lugs require nuts and bolts to attach them to the Transformer terminals
Resolution:
The components of the kit (including the hardware) are not available on an individual basis from SquareD/Schneider Electric. Refer to Digest 178 Page 14-9 Transformer Lug Kits table. This table lists the quantity and size of hardware supplied, which can be obtained at any local supply store.
The following video describes the contents of the DASKGS250 & DASKGS400 Transformer Lug Kits:
Released for: Schneider Electric USA