Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What gauge of steel is used for the covers, front, sides & back the QED NEMA 1 Switchboards?
Issue:
Thickness of sheet metal used in our QED NEMA 1 Switchboards

Product Line:
QED Switchboards

Environment:
Product Features

Resolution:
Steel thickness for SQ D Nema 1 SWBD's 14 gauge

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings