Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the standard bus material for an NF Panelboard?
Issue:
What material is used for the bussing in NF panels?

Product Line:
Panelboards

Environment:
NF Panelboards

Resolution:
NF panelboards use tin plated aluminum with tin plated copper branch connectors.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings