Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference in how the watt-hour meter installs into the socket of the EZMK vs EZML branch devices?
Issue:
Product Design features

Product Line:
EZM metering equipment

Resolution:
The EZMK devices use a meter socket that is called a K-base socket. This means that the watt-hour meter BOLTS into place.
The EZML devices use a meter socket that is called an S-base socket. This means that the watt-hour meter PLUGS into jaws of the socket.

NOTE: It is ALWAYS IMPORTANT to check with the local electric utility company for approval, BEFORE obtaining and installing metering equipment.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings