Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the conductor temperature rating for the Homeline breakers?
Issue:
Product Design Features

Product Line:
Miniature Circuit Breakers

Resolution:
The 40 - 125 A Homeline breaker lugs are all rated at 75 degrees C. 90°C conductors may be used if installed in accordance with the 75 degree C wire tables of the current NEC (National Electrical Code).
The 15 - 35 A Homeline breaker lugs are dual rated 60/75 degrees C.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings