Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the flange mounted variable depth operating mechanism for H and J frame breakers?
Issue:
Flange mounted variable depth operating mechanism compatible to H and J frame breakers.

Product Line:
Circuit Breakers

Environment:
Powerpact H and J frame breakers

Cause:
N/A

Resolution:
Catalog number is 9422RQ1. Variable mounting depth range: 5.88 inches to 17.75 inches.

Note:
If the handle is also needed, then one of the following will need to be ordered along with operating mechanism.

6-inch Handle Mechanisms:
  • Cat#: 9422A1 (Nema 1, 3, 3R, 4 and 12)
  • Cat#: 9422A2 (Nema 4 and 4X)
4-inch Handle Mechanisms:
  • Cat#: 9422A3 (Nema 1, 3, 3R, 4 and 12)
  • Cat#: 9422A4 (Nema 4 and 4X)

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings