{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Why am I not getting any output voltage on an XUK0ARCTL2 photo electric sensor?<br /><br />
The output relay of this sensor is dry. No output will be produced until voltage is applied to the relay common. There is an error in the wiring diagram on pg. 53 in the Solid State Sensors catalog Doc. # 9006CT0101. Correct colors are BRN = L1 or DC positive, BLU = L2 (neutral) or DC common, GRY = relay common, BLK = N.O. contact, WHT = N.C. contact.


CTA-ID : 2031492

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.