What is the part number for the adapter included with XCKT and XCKP limit switches that goes from metric to 1/2`` NPT?<br /><br /><br />
DE9RA1012 is the adapter. Be aware that this unit is not required on the new Osiswitch products. The cable entry adapter can be changed out without affecting the dimensions of the device. On the ZCP21, for example, ZCPEN12 is the conduit entry for 1/2 inch NPT threads.
CTA-ID : 2033030
CTA-ID : 2033030
Released for: Schneider Electric USA
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales inquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.