This is a mirror assembly that mounts on an 18mm barrel photo sensor to turn the beam 90 degrees. Obsolete, as is the XUBZ01. Superior product available with mirror sealed inside sensor. [e.g. XUB9BPAWM12]. The ``W`` in the part number codes for 90 degree sensing. Many models are available.
Released for:Schneider Electric USA