Issue:
Can you put a control wire on Powerpact H and J frame breakers?
Product Line:
Molded Case Circuit Breaker
Resolution:
The part number is S37423 for the H frames and S37424 for the J frames.
Each control wire terminal has a 1/4 in. (6.3 mm) male spade connector tab which allows monitoring of circuit status.

See instruction bulletin 48940-233-01.
Can you put a control wire on Powerpact H and J frame breakers?
Product Line:
Molded Case Circuit Breaker
Resolution:
The part number is S37423 for the H frames and S37424 for the J frames.
Each control wire terminal has a 1/4 in. (6.3 mm) male spade connector tab which allows monitoring of circuit status.
See instruction bulletin 48940-233-01.
Released for: Schneider Electric USA