Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for a CM200S, series M02?
Issue:
Repair parts

Product Line:
CSED

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4053414150
Main Breaker Section Cover Assembly - 7329410550
Main Breaker Section Cover Hinges - (2) X2983
Main Breaker Section Cover Hinge Mounting Screws - (2) 2159414081
Dead Front Interior Trim - 7329420101 (also requires insulator and rivets, below)
Dead Front Interior Trim Insulator - 4053435601 (attaches to rear of interior trim)
Dead Front Interior Trim Insulator Rivets - (2) 2430313230
Dead Front Interior Trim Danger Label 4027370902
Dead Front Interior Trim Mounting Screw - 4020513001K (contains 10 screws; only one screw is required to secure the trim)
Meter Base Assembly - 4053448450 (includes meter base, (2) line side lugs, (4) meter jaws, and (4) meter jaw blade guides and load side bussing)
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Nuts - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Left Line Side Lug Assembly - 4053408750
Right Line Side Lug Assembly - 4053408850
Meter Sealing Ring - 2920910001
Closing Cap - (2) ACP
Main Breaker - QOM2-VH type, 200 A maximum
Main Breaker Mounting Nuts - (2) 2342702001
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings