{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can a Motorlogic overload be set to auto reset after a trip?
Issue:
Does the Motor Logic overload have the feature for auto reset after a trip?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Class 9065 Motor Logic Solid-State Overload Relays

Resolution:
Only if the remote reset accessory is used with an external timer.

Schneider Electric USA