How can we help you today?

What is the torque value needed for the 1/2"-13 VISI-TITE Nut used in EZM for connecting the horizontal cross buss together after the outer head has been broken off?

Issue:
Product Design Features

Product Line:
EZM Metering

Environment:
Main Horizontal bus connection nut

Cause:
Installation

Resolution:
50 lb.-ft. of torque is required for the inner hex head nut once the outer head of the VISI-TITE nut has been removed. This information is also provided on the wiring diagram of the EZM device.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings