How can we help you today?

What are the repair parts for a QUM400CK, Series M01?

Issue:
Repair parts

Product Line:
Combination Service Entrance Device

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056247750. This is a one piece Meter Cover/Utility Pullbox Cover.
Meter Cover Mounting Screws 4020513001K and (3) Sealing Screw X1299
Main Breaker Section Cover - 4056258950
Main Breaker Section Cover Mounting Screws - (3) 2142217101
Utility Pullbox Cover - See Meter Cover, above.
Utility Pullbox Cover Handles - The Meter Cover is not supplied with handles.
Interior Deadfront Trim - 7329420650
Interior Deadfront Trim Mounting Screws - 4020513001K (10 screws in kit, only 6 used to mount trim)
Interior Deadfront Trim Handle - (1) 2940101103 and Rivets (4) 2430315290
Meter Base Assembly - 58763-4 and 58764-4
Mounting Channel - 4056142003
Factory Installed Main Breaker - DGP36400E20LH (Obsolete and no longer available. Can be replaced with LJL36400U31X. Mounting Kit S36967 is also required. The lugs on the ON end of the breaker must be removed for connection to the busbars. The B phase (center) lug should also be removed from the OFF end of the breaker.
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings