{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can you stack the ZBE1015 or ZBE1025 contact blocks?
Issue:
Can Spring terminal blocks be stacked?

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony XB4/XB5 Push buttons

Resolution:
Additional blocks cannot be attached to the back of these contact blocks. However, spring terminal contact blocks can be mounted behind screw terminal contact blocks.

Schneider Electric USA