Can an NQMB4LA main breaker adapter kit be used with either a two pole or three pole main breaker?
Issue:
Can an NQMB4LA be used with either a two pole or three pole main breaker?
Product Line:
Panelboard
Environment:
NQ Panelboard
Resolution:
The NQMB4LA main breaker adapter kit can use either a 2 or 3 pole breaker ``LAL`` or ``LHL`` type breaker frame. For example, an LAL26400 for the two pole, or an LAL36400 for the three pole.
See attached Instruction Bulletin
Can an NQMB4LA be used with either a two pole or three pole main breaker?
Product Line:
Panelboard
Environment:
NQ Panelboard
Resolution:
The NQMB4LA main breaker adapter kit can use either a 2 or 3 pole breaker ``LAL`` or ``LHL`` type breaker frame. For example, an LAL26400 for the two pole, or an LAL36400 for the three pole.
See attached Instruction Bulletin