Issue:
Do the ATS01 come with overload protection?
Product Line:
ATS01
Environment:
Products sold and used in the United States
Cause:
NA
Resolution:
No. Motor overload protection must be provided separately. Solid state overload devices are not compatible with these softstarters. It is recommended to use bimetal or thermal magnetic type overloads instead.
CTA-ID : 2049410
Do the ATS01 come with overload protection?
Product Line:
ATS01
Environment:
Products sold and used in the United States
Cause:
NA
Resolution:
No. Motor overload protection must be provided separately. Solid state overload devices are not compatible with these softstarters. It is recommended to use bimetal or thermal magnetic type overloads instead.
CTA-ID : 2049410
Released for: Schneider Electric USA