Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are Square D panelboards available in a Type #316 Stainless Steel enclosures?
Issue:
Panelboards in a Type #316 Stainless Steel enclosures

Product Line:
Panelboards

Environment:
Panelboard enclosures sold and used in North America

Resolution:
Yes. NQ,  NF, and I-Line type panels are available in Type #316 Stainless Steel enclosures.
Reference the current  Supplemental Digest for further information. Add 25% to the #304 stainless steel prices shown.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings