Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the repair parts for the H322DS, series F5 (F05)?
Issue:
Field replaceable parts for H322DS series F05 / F5

Product Line:
Safety Switch

Environment:
Heavy Duty Safety Switch

Resolution:
The repair parts for the H322DS, series F5 (F05) are as follows. No other parts are available.
-Line Base Assembly - 4056642950 (arc suppressor not included)
-Load Base Assembly - 4056002750
-Line & Load Base mounting screw - 4020516001 (3 for line & 2 for load)
-Arc Suppressor Assembly - HAS0610F (includes arc suppressor and mounting screw)
-Lug Assembly - CL0306F (includes 6 lugs)
-Mechanism Assembly - 4056610750 (NOTE: Handle Coupling, Cover Interlock Defeat Coupling, and Lockplate Gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056699450 (also recommend replacing Lockplate Gaskets)
-Lockplate - 4056693201 (also recommend replacing Lockplate Gaskets)
-Lockplate Gasket - 4050322803 (2 required)
-Lockplate mounting screw - 2194900101 (2 required)
-Ground Lug - 4025101652 - (2 total required)
-Ground Lug Mounting Screw - 4020513503
-Fuse Pullers - FPK03 (1 required for switch)

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings