Issue:
Product Design
Product Line:
MP Meter Pak
Environment:
Product availability
Cause:
Product Features
Resolution:
Square D does NOT offer a 5 or 6 position, Ringless MP with Lever Bypass. The maximum number of meters with Lever Bypass would be 4 positions. Consider using the EZM Metering equipment for applications that require more than 4 meter sockets with Lever Bypass.
Product Design
Product Line:
MP Meter Pak
Environment:
Product availability
Cause:
Product Features
Resolution:
Square D does NOT offer a 5 or 6 position, Ringless MP with Lever Bypass. The maximum number of meters with Lever Bypass would be 4 positions. Consider using the EZM Metering equipment for applications that require more than 4 meter sockets with Lever Bypass.
Released for: Schneider Electric USA