Issue:
Needs to know if the ring that is used to hang up the pendant station a standard feature of the XACA960
It is the piece that can be found between the (2) XACB961 screws at the top part of the XACA960.
Product Line:
Push Buttons and Operator Interface
Environment:
Pendant Stations
Resolution:
Yes the ring used to hang up the pendant station is a standard feature for all the XACA pendant stations.
Needs to know if the ring that is used to hang up the pendant station a standard feature of the XACA960
It is the piece that can be found between the (2) XACB961 screws at the top part of the XACA960.
Product Line:
Push Buttons and Operator Interface
Environment:
Pendant Stations
Resolution:
Yes the ring used to hang up the pendant station is a standard feature for all the XACA pendant stations.
Released for: Schneider Electric USA