What is the S suffix on the ATV212HD22N4S drive?
Resolution:
The "S" suffix in ATV212HD22N4S stands for Slim Version. This model has a more compact physical design and reduced dimensions compared to the standard ATV212HD22N4.
Because of its smaller enclosure size, the ATV212HD22N4S has different thermal characteristics. To maintain reliable operation, the drive is limited to a 6 kHz switching frequency for continuous operation at 40°C ambient temperature.
Additionally, the compact design results in higher power dissipation at nominal current compared to the standard ATV212HD22N4. As a result, special attention should be given to installation conditions, ventilation requirements, and derating considerations.
If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:
Frequently Asked Questions - Schneider Electric (se.com)
If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.
If you are not located in North America, please contact your local Customer Care Center for assistance: