Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
On the NQ type panelboards that are suitable for use as service entrance, what precautions/steps are taken to prevent additional breakers from being added to the panel?
Issue:
Precautions taken to prevent additional breakers from being added to the NQ type panelboards that are suitable for use as service entrance

Product LIne:
PTFDS FD  Enclosure Systems

Environment:
NQ panelboards sold and used in North America

Cause:
Can additional branch breakers be added to a service entrance NQ panelboard?

Resolution:
Factory Assembled panels have non-reversing screws installed in the unusable branch connectors to prevent additional breakers from being installed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings