Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What circuit breaker types will an QMBJW, QMB branch circuit breaker unit accept?
Issue:
Circuit breakers used in the QMBJW

Product Line:
QMB panelboard, switchboard with QMB distribution.

Environment:
Products sold and used in North America

Cause:
Not all of the PowerPact J frame breakers should be used in the QMBJW.  The JJA and JLL types are not listed for use in the QMBJW.

Resolution:
The QMBJW will accept the 150A to 225A JDL and JGL type circuit breakers. as stated in the QMBJW labels.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings