Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can feeder conduit be fed up through the bottom of Ventilated and Non Ventilated Transformers?

Issue:
Conduit entry for Ventilated and Non Ventilated Transformers

Product Line:
LV Transformers

Environment:
Applies to Ventilated and Non Ventilated Transformers by SquareD/Schneider Electric

Cause:
Ventilated and Non Ventilated Transformers have an allowable wiring area, below the terminal strip, shown on the CAD drawing


Resolution:
Yes, Customer can punch holes in the bottom pan and conduit stub-up to it as needed.  The left and right front sides of the transformer enclosure, below the terminal strip are also an allowable area.  Conduit entry is restricted to the crosshatched wiring area shown on the drawings.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings