Browse FAQs

VAMP RS-485 communications adapter module

Published date: 11 June 2020

Issue  
Need to communicate RS-485 but it cannot be ordered for the VAMP.

Product Line  
VAMP

Resolution  
The VSE 002 is an internal RS-485 module that is used to connect the VAMP protection relays to a RS-485 bus. Additionally this module may be used with any device which has an RS-232 or TTL serial interface when an RS-485 interface is required. Please see the attached document for more details.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.