How can we help you today?

What are the repair parts for a QUM400CK, Series M02?

Issue:
Repair parts

Product Line:
Combination Service Entrance Device

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
Only the parts listed below are considered field replaceable.
Meter Cover - 4056247750. This is a one piece Meter Cover/Utility Pullbox Cover.
Meter Cover Mounting Screws 4020513001K and (3) Sealing Screw X1299
Main Breaker Section Cover - 4056258950
Main Breaker Section Cover Mounting Screws - (3) 2142217101
Utility Pullbox Cover - See Meter Cover, above.
Utility Pullbox Cover Handles - The Meter Cover is not supplied with handles.
Interior Deadfront Trim - 7329420650
Interior Deadfront Trim Mounting Screws - 4020513001K (10 screws in kit, only 6 used to mount trim)
Interior Deadfront Trim Handle - (1) 2940101103 and Rivets (4) 2430315290
Meter Base Assembly - 58763-4 and 58764-4
Mounting Channel - 4056142003
Factory Installed Main Breaker - LJL36400U31X. Mounting Kit S36967 is also required. The lugs on the ON end of the breaker must be removed for connection to the busbars. The B phase (center) lug should also be removed from the OFF end of the breaker.
Utility Lug Mounting Hardware - 4056211850
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings