Issue:
When user saves the Powerlink Configuration in LCS Basic or Advanced version 1, LCS gives "Path Error" stating that it can not save the file.
Product Line:
Powerlink Lighting Controls
LCS Basic or Advanced software
Environment:
Running LCS Basic or LCS Advanced version 1 on Windows 7 or 8.
Cause:
User is not an administrator on the computer. Windows does not allow the non-Administrators to save to the Program Files path which is the default save location for LCS.
Resolution:
Change the file location for LCS. Follow procedure in the attached document.
When user saves the Powerlink Configuration in LCS Basic or Advanced version 1, LCS gives "Path Error" stating that it can not save the file.
Product Line:
Powerlink Lighting Controls
LCS Basic or Advanced software
Environment:
Running LCS Basic or LCS Advanced version 1 on Windows 7 or 8.
Cause:
User is not an administrator on the computer. Windows does not allow the non-Administrators to save to the Program Files path which is the default save location for LCS.
Resolution:
Change the file location for LCS. Follow procedure in the attached document.