Issue:
Standard Terminal Lug Data
Product Line:
EZM Metering
Resolution:
The EZM12000TB and EZM32000TB main terminal boxes both come with a lug landing pad and do not have lugs standard from the factory. Each device will accept as standard (6) lugs per phase and neutral. See attached drawings for approved lugs to use.
Standard Terminal Lug Data
Product Line:
EZM Metering
Resolution:
The EZM12000TB and EZM32000TB main terminal boxes both come with a lug landing pad and do not have lugs standard from the factory. Each device will accept as standard (6) lugs per phase and neutral. See attached drawings for approved lugs to use.
Released for: Schneider Electric USA