How can we help you today?

What is the option card part number that has a combination modbus TCP/IP and Ethernet IP?

Resolution:

The option card that supports both Modbus TCP/IP and EtherNet/IP communication protocols for the ATV61 and ATV71 drives is the VW3A3320 Ethernet communication card.

The VW3A3320 allows the drive to communicate over Ethernet networks and supports:

  • Modbus TCP/IP
  • EtherNet/IP

This card can be installed in compatible ATV61 and ATV71 drives to provide network connectivity for PLCs, HMIs, SCADA systems, and other Ethernet-based control systems.

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)


Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings