How can we help you today?

How to configure a ION6200 device from the front display

Issue
Need to enter setup mode or configuration mode of an ION6200

Product Line
ION6200

Environment
Installation or setup a power meter.

Cause
Entering configuration mode on a ION6200 is not clear.

Resolution
ENTER Configuration Select mode by pressing the Up and Down buttons at the same time and holding for 2 seconds.
ION 6200 ION6200 Setup Configuration Menu

Use the arrows to toggle through the settings and use the white circle button to enter edit for a parameter.

ION 6200 ION6200 Setup Configuration Mode Front Display

See page 19 in the attached document for information on setup parameters.

Schneider Electric USA

Attachment(s)
ION 6200 User Guide.pdf [1.62 MB]
Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings