{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
How can we help you today?
Can C/C++ program stop/interrupt TelePACE Ladder Logic in SCADAPack when event occurs?
The runTarget() function is available for the customer, but the intention of this is to turn off the logic application on power up when they have no need to use logic.  It is not intended to be used as a throttle mechanism. This is not how SCADAPack firmware architecture works.  Ladder logic will complete full cycles.  It may be interrupted by higher priority tasks, but it does not have the ability to signal a higher priority task to take over.

Schneider Electric USA

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.