Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a 100% rated mission critical breaker an option for the Main breaker on a NQ 225 amp Panels?
Issue:
Use of 100% rated mission critical breaker as a Main breaker on a NQ 225 amp Panels

Product Line:
NQ Panelboard

Environment:
Application

Cause:
Product Features

Resolution:
We have not tested NQ , or NF Panles with 100% Mission critical breakers and have no alternative since JDL Mission cruitical breakers cannot be installed into a seperate J250S enclosure

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings