Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What size strip heater is used in our NQ, NF, I-line, and combo I-line panelboards?
Issue:
Size strip heater used in NQ, NF,  I-line, and combo I-line panelboards

Product Line:
Panelboard strip heaters

Environment:
NQ, NF, I-line, I-line combo

Cause:
Clarification on sizing

Resolution:
Panelboards utilize the 120V 200W size strip heaters. Strip heaters are only available as a factory assembled option and are not sold separately, nor available as a Field installed option.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings