How can we help you today?

How do I send a start/stop and a speed command to the Altivar Process Drive over Ethernet (Modbus TCP) protocol?

Resolution:

To send Start/Stop commands and a speed reference to an Altivar Process Drive over Ethernet using Modbus TCP, configure the drive according to the desired control profile.

Unit ID 1

When not using the I/O Scanner, set the Modbus Unit ID to 1.

On the drive:

[Communication] → [Comm Parameters] → [Modbus SL] → [Modbus Fieldbus]

  • Set Modbus Address = 1

CiA402 / DRIVECOM Profile

Go to:

[Complete Settings] → [Command and Reference] → [Control Mode] (CHCF)

Set CHCF to:

  • [Not Separ.], or
  • [Separate Mode]

The drive will follow the CiA402 profile, referred to as DRIVECOM on older products.

Command Word Register: 8501

To start the drive, write the following decimal values to register 8501 in sequence:

6 → 7 → 15

After initialization:

  • 7 = Stop
  • 15 = Run

I/O Profile

If CHCF is configured for I/O Profile, use the following settings:

[Communication] → [Comm Parameters] → [Modbus SL] → [Modbus Fieldbus]

  • Set Modbus Address = 1

[Complete Settings] → [Command and Reference] → [Control Mode] (CHCF)

  • Set to [I/O Profile]

Registers:

  • 8501: Command Word, 16-bit
  • 8502: Frequency Reference, 0.1 Hz units
  • 8602: Speed Reference, 1 rpm units

To start or stop the drive under I/O Profile, toggle Bit 0 of command word 8501.

Once the run command has been sent, provide the speed reference by writing to:

  • 8502 for frequency in 0.1 Hz increments, or
  • 8602 for speed in 1 rpm increments.

When using register 8602, make sure [Nominal Motor Speed] is correctly configured in the [Motor Parameters] menu.

Unit ID 255 - I/O Scanner

When using the I/O Scanner, use Unit ID 255.

  • The Modbus Address can remain at 0.
  • Enable the I/O Scanner through SoMove.
  • The drive will then use the configured I/O Scanner input/output tables.

For additional configuration details, refer to the FAQ “How do I enable and configure the I/O Scanner on the Altivar Process Drive?”.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings